11/10/2008 6:18 AM | |
Joined: 11/9/2008 Last visit: 7/11/2024 Posts: 404 Rating: (6) |
Dear Can u tell me basic deffrence between Software and Hardware Redanduncy? i'm Wattting for ur reply. |
11/12/2008 2:39 PM | |
Joined: 11/9/2008 Last visit: 7/11/2024 Posts: 404 Rating: (6) |
Hi H-H Thanks for ur reply. Regadrs, YogendraG |
11/12/2008 2:39 PM | |
Joined: 11/9/2008 Last visit: 7/11/2024 Posts: 404 Rating: (6) |
HiAnman Elotaify, Thanks for ur reply. Regadrs, YogendraG |
4/19/2009 5:18 PM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306) |
this is just tocorrect inaccurate information, In software redundancy, not only ET200M that can be used but also the ET200iSP (redundant IM152-1 with firmware version > 2.0 ) Although it hasn't been mentioned yet in SWR manual orlatest software versionbut according to the ET200 iSP manual and the available firmware versions, it is possible to configure software redundancy with ET200iSP. I also would like to comment on what Mr. Ayman said regarding Y-Link and ET200M
This is not quite accurate. I had a discussion with Siemens staff before and they said it's not recommended at all to use ET200M after a Y-Link. I also had a discussion with ET200iSP tehc. support and said the same, it's not recommended to use ET200iSP after Y-Link. It is possible but not recommended. The Y-Link isa solutionfor DP-Slaves with single DP port but for ET200M and ET200 iSPit should be2 interface modules in each remote rack. Best regards. H-H AttachmentSWR & ET200 iSP.pdf (449 Downloads) |
This contribution was helpful to2 thankful Users |
7/11/2014 3:28 PM | |
Joined: 9/1/2005 Last visit: 7/9/2024 Posts: 4101 Rating: (194) |
follow up question published by ALUis split to a seperate thread with the subject H-system for S7-300 or S7-1200?. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on