12/14/2015 1:51 PM | |
Posts: 4 Rating:
|
I have TIA portal V13 SP1 update 5, Step7 Pro V13 SP1 update 5 and WinCC Advanced V13 SP1 update 5 installed only on my VM Does PLC SIM require the other software packages (listed in link below) in order to operate Do I need to install SCOUT TIA, Safety V13 etc as listed in http://support.automation.siemens.com/WW/view/en/105825934 Safety V1 or do you only have to update the packages if you have them previously installed? I have installed Step 7 PLCSim however it is coming up with errors when I attempt to open it. (See attached screenshot) ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/15/2015 11:25:24 AMNew subject after splitting |
|
12/14/2015 2:11 PM | |
Posts: 5225 Rating:
|
To make a long story short...
|
12/15/2015 11:43 AM | |
Joined: 7/9/2015 Last visit: 7/18/2024 Posts: 3875 Rating:
|
Hi,
yes, do like William told. Look to this FAQ ...
Why can you no longer start PLCSIM V13 SP1? https://support.industry.siemens.com/cs/de/en/view/109479634
Towome
|
|
|
Follow us on