11/22/2021 5:47 AM | |
Joined: 1/11/2019 Last visit: 9/10/2024 Posts: 758 Rating: (149) |
Hi Phuoccd, 1. Ideally, they have to be same OS, same configuration Even the information system suggests the same 2. Time Synchronization. You have to do the Time synchronization in order to get the alarms in same time stamp between AS, OS and clients. Please go through the below link to configuring the Time Synchronization PCS 7 Time Synchronization (V9.0 SP2) P lease go to page number 39 (Section 4.3 Configurations for time synchronization in a work group) Hope it helps you :) |
This contribution was helpful to1 thankful Users |
Follow us on