9/14/2019 9:39 AM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
Use EPos in MDI mode. Then you can change between Setup (like jog) and absolute Positioning on the fly |
9/15/2019 8:06 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (875) |
Hello, For CU 391, For ALM = 999, For DO = 138 or 136 depends on drive application. HTH |
9/16/2019 7:26 AM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (296) |
Hi, I would recommend telegram 20 or 352 for the Servo DO - there are also ready to use SIMATIC FBs for those telegrams (LSINAExt lib): https://support.industry.siemens.com/cs/ww/en/view/109747655 But here you do not have a position feedback, I do not really understand why you need the position of the spindle? You just want to do speed control so a position is not relevant usually for that type of control. |
Best regards, |
|
Follow us on