Industry Online Support
Technical Forum
1/5/2012 12:33 AM | |
Posts: 7 Rating: (0) |
DearSir/Madam, We have a problem here on 8 units of MM430 ranging from 7.5kW to 15kW, always trip on F0022 sporaically during normal operation. Theytrip like every few weeks and can be reset.It is being used in water pump application. Is there any possibility of MM430 being not optimisedbecause wedid not do any motor ID since using V/f control (P1300=2)? Any possibility on product quality on this particular batch of MM430?
AttachmentParameter List.zip (223 Downloads) |
1/5/2012 5:23 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477)
|
There was a lot of discussion here about this fault You can refer and those might be useful to you. Use search function to find same.. Here are some reference threads for you /tf/WW/en/Posts/49487 /tf/WW/en/Posts/41667 /tf/WW/en/Posts/7328 If you still facing problem, then come back again and share your checks and observation so that you can get better help Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on