12/8/2013 8:27 AM | |
Joined: 8/27/2006 Last visit: 9/24/2024 Posts: 719 Rating: (88) |
Dear All, I have a project where I need to migrate S5 to S7 for a boiler's process PLC. The boiler is controlled through 9 DR22 controllers and 3 DR24 controllers. My PLC is connected to them via Profibus. I have the uploaded software (without symbols) so I try to understand it to program its equivalent in S7. I have attached the program with this post The question is: I'm stuck at understanding FC22, 23, 24 and 25 FC22'n name is DR22 FC23's name is DR22/2 FC22'n name is DR24 FC23's name is DR24/2 If anyone can tell me what do these function do I'll be very grateful.
Attachmentprocess.zip (241 Downloads) |
The more you know, The more you know that you don't know |
|
12/11/2013 6:16 PM | |
Joined: 12/1/2009 Last visit: 9/5/2024 Posts: 672 Rating: (147) |
Salam AMAZINGAHMED , some nice function blocks do you have. They are protected and seam to be part of a standard package, but not neccesary. In general they are for communicatingbetweenthe SIPART's andthe IM308C. I don't see that much use for you to understand them in detail, while in S7 you communicate different and easier. The most important for youto find out is which data is/must begetting transferred. Do you have any experiencein communicating between S7 and SIPART? Kindly contact me by PM so that I can give you a hand. Best Regards. |
Give us your feedback and show us your respect! |
|
Follow us on