4/15/2016 9:21 AM | |
Joined: 9/12/2007 Last visit: 8/24/2020 Posts: 12 Rating: (0) |
Hello, In one single project, 7 PLC are configured. Until recently, the cross reference is not working in two of the PLC program blocks. From the error codes, I can refer to the S7 error codes and the remedy actions. Therefore the project reorganization is performed but it doesn't help much. Three screenshots are attached in this topic and I hope you can help to advise if there are other way to resolve this issue. Thank you. Attachmentscreenshots.zip (231 Downloads) |
4/15/2016 9:54 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:50:43 AM~(‾▿‾)~ |
|
Follow us on