3/20/2014 8:02 AM | |
Posts: 2930 Rating: (432)
|
Hi, in LSC open your program, then goto File/Save AS, then: Select "Binary dump (*.bin) as file type. The file name MUST be LOGO_U_P. Stor the file directly on the SD-Card, or send this file without changing file name to sombody, let him copy this file to a SD-card and then you can use this sd-card to program LOGO! 0BA7. See the attached example: Hope this helps AttachmentLOGO_U_P.zip (224 Downloads) |
This contribution was helpful to1 thankful Users |
3/20/2014 8:12 PM | |
Posts: 158 Rating: (1) |
ok seems to work fine via 'card' menu. You must have the correct LOGO selected in program (Standard vs. logo 7ES1)... |
3/21/2014 1:07 PM | |
Posts: 2930 Rating: (432)
|
Hi, don't remove or plug in the card while LOGO! is in RUN. Always do a RUN/STOP/RUN. Regards |
Last edited by: Helmut_13 at: 3/21/2014 1:08 PM |
|
3/21/2014 4:20 PM | |
Posts: 158 Rating: (1) |
thank you guys! working great! |
This contribution was helpful to1 thankful Users |
Follow us on