5/3/2020 1:59 PM | |
Posts: 2 Rating: (0) |
Hello Daniel Chartie, I have another problems with the syn module configuration for CPU 414-5H by HW Config Editor in Simatic Manager. 1) I have selected the above CPU and tried to add the sync module. In general, the available slot will show green color when I select the component, However, it didn't when I select the sync module under the same CPU. The screen capture is attached. Please comment and thanks. 2) I also want to duplicate another set of CPU 414-5H for redundant configuration by copy and paste but it doesn't work.The screen capture is attached. Please advise how I can configure it and thanks. FYI. I am using HW Config Editor of Simatic manager and I installed STEP 7 Professional 2017 V5.6 + HF1 software. Would you please help? Thanks and best regards RL
------------------------------------------------------------------------------------------ |
Last edited by: RingoL at: 05/03/2020 14:01:18Last edited by: RingoL at: 05/03/2020 14:01:26Last edited by: RingoL at: 05/03/2020 14:01:31Last edited by: RingoL at: 05/03/2020 14:02:17Last edited by: RingoL at: 05/03/2020 14:02:32Last edited by: RingoL at: 05/03/2020 14:02:47Last edited by: RingoL at: 05/03/2020 14:02:55Last edited by: RingoL at: 05/03/2020 14:03:37Last edited by: Jen_Moderator at: 05/04/2020 11:36:31New subject after splitting |
|
5/3/2020 2:06 PM | |
Posts: 2 Rating: (0) |
Attachment1) Not able to insert sync module to IF1 or IF2 in HWConfig of Simatic Manager.jpg (182 Downloads) |
Follow us on