2/9/2015 8:53 PM | |
Posts: 3 Rating: (0) |
Hi Pittiplatsch, besides the remote control of ports via WBM or line command, are there any telegrams that can be used to enable/disable the ports of a X208pro scalance out of the S7 code? I have a S7-1500 and would need to enable/ disable ports on the scalance switch from the program. Is this a feature that is already in place? Thanks for the help in advance.
--------------- |
Last edited by: Min_Moderator at: 2/10/2015 3:05:34 PMNew subject after splitting |
|
2/10/2015 3:21 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on