Industry Online Support
Technical Forum
2/9/2009 3:36 AM | |
Joined: 9/27/2006 Last visit: 11/14/2024 Posts: 12294 Rating: (2691)
|
Hello; Siemens has implemented some specialized temperature PID controllers in Step 7, FB58 and FB59. For your application you should study FB58, "TCONT_CP", a continuous control algorithm that allows a pulse duration modulation output for the control of heatingelements (SCRs). Manual on Temperature PID controller FB58: http://support.automation.siemens.com/WW/view/en/18652438 Thread on the forum discussing typical implementation problems of FB58: /tf/WW/en/Posts/19163Hope this helps, Daniel Chartier |
Follow us on