6/11/2024 11:36 AM | |
Joined: 1/21/2013 Last visit: 7/26/2024 Posts: 3023 Rating:
|
Hi youssouf-attia, In the technical data you will find the following: Number of distributed IO systems 32; A distributed I/O system is characterized not only by the integration of distributed I/O via PROFINET or PROFIBUS communication modules, but also by the connection of I/O via AS-i master modules or links (e.g. IE/PB-Link) This means you can use up to 32 fieldbus systems with PROFINET, PROFIBUS, AS-i. This is unlikely to be achieved with your planned system as you are likely to use only one IO system for PROFINET by using the internal interface as the PROFINET IO controller. You can connect up to 128 PROFINET IO devices and you have listed 40 because the TP1200 Comfort is not normally used as an IO device. Kind regards |
Follow us on