9/30/2019 4:33 PM | |
Posts: 1 Rating: (0) |
good morining The simatic IoT 2040 device is compatible with Siemens S7 200 and 300 PLCs |
9/30/2019 5:45 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Yes, you can e.g. use an S7-Connection to read/write values to the PLC. For the S7-200 you will need an additional CP 243-1. You can find more information in this thread. Another possibility would be to use Modbus-RTU. Haven't tested that with an S7-200 so far, but it should work. Kind regards! |
Follow us on