8/21/2015 3:05 PM | |
Joined: 5/7/2013 Last visit: 1/3/2023 Posts: 16 Rating: (2) |
Hi All, I'm have problems with starting Tia Portal.. my computer locked up when I had Tia portal open.. From that point on it will not start up again.. at this point I do not have access to the original Install dvd's to reinstall.. Also the last update 5 is also installed via internet so it will not restart.. I have added a PDF from the error report can any one help me please.. Keith AttachmentTia V13 Sp1 ErrorRep.pdf (231 Downloads) |
8/21/2015 3:26 PM | |
Joined: 5/7/2013 Last visit: 1/3/2023 Posts: 16 Rating: (2) |
Hello Christoph, My original installation was Tia12 and have done the updates all the way through.. the last few times via the automatic updater.. Here is also the full error report Thanks for your prompt reply Yours Keith Attachmenta4339ebe-fa8a-4ca8-ac41-b8cb2f38d887.zip (190 Downloads) |
Last edited by: Laarmann at: 8/21/2015 3:28:14 PM |
|
8/21/2015 3:32 PM | |
Joined: 5/7/2013 Last visit: 1/3/2023 Posts: 16 Rating: (2) |
Hello Christoph, I will try again it should be with attached with the message.. a4339ebe-ect ect Attachmenta4339ebe-fa8a-4ca8-ac41-b8cb2f38d887.zip (197 Downloads) |
8/21/2015 3:39 PM | |
Joined: 5/7/2013 Last visit: 1/3/2023 Posts: 16 Rating: (2) |
Hello Christoph, Yes it is available it is 4Kb and the time stamp is 8-7-2015 14:37 Yours Keith |
8/21/2015 4:02 PM | |
Joined: 5/12/2006 Last visit: 10/11/2024 Posts: 22410 Rating: (3017) |
Hello, can you post the MPK here? Christoph |
8/21/2015 4:07 PM | |
Joined: 5/7/2013 Last visit: 1/3/2023 Posts: 16 Rating: (2) |
Hello Christoph, Here it is I had to zip it.. thanks keith AttachmentStep7.Package.BasicMotionControl.zip (198 Downloads) |
Follow us on