1/30/2017 2:02 PM | |
Posts: 111 Rating: (16) |
Hello, first question: TIA portal is more a PLC system for local or small automation. The focus is more on the high speed of controlling. PCS 7 is more a DCS system for decentralized and bigger automation. The focus is more on the high availability/redundancy of the system. But in the end, for the most things both systems are the same. There are only differents in the details like, kind of CPU, kind of redundancy, numbers of I/O,... ==> Today there is no strong splitting between PLC and DCS. More information about the S7-1200 you can find here: https://support.industry.siemens.com/cs/ww/en/view/109741593 second question: There are some information about the standard architectures in PCS 7, which could help you to decide if you shall use PCS 7 and which architecture: https://support.industry.siemens.com/cs/ww/en/view/109739629 Hopefully I could held you. |
This contribution was helpful to3 thankful Users |
Follow us on