1/10/2013 10:41 AM | |
Posts: 2 Rating: (0) |
Hi, I am working on a project with TIA WinCC Comfort . The Panel is TP1200 Comfort. While compiling, it gives an error an it's written "the application has encountered a problem and needs to close" on the pop up. I had this error many times while working on. Its really bad situation that i need to close the programme in the middle of the working, couldnt see and fix the problem. its wasting my time. I curious about that if i do something really wrong. For example; is it a problem to have simatic manager, wincc v7 sp3 and also TIA Portal on the same pc? is it because i have this error pop up too many times when i add any little new things to my program like trends or alarms? thanks for help serpil
AttachmentTIA ERROR.zip (99 Downloads) |
1/10/2013 11:39 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hi, If you have latest update for SP2 which is Upd5 and it still generates an error then I think best idea is to open support request case. The guys from support will investigate what's wrong. If you worry about comaptibility then look hereWhat should you watch out for when installing STEP 7 (TIA Portal) V11? Also I believe that there is no SP3 for WinCC v7.0. The latest is Upd10 for SP2 WinCC v7.0
|
Best regards, |
|
12/30/2013 11:16 PM | |
Joined: 9/1/2005 Last visit: 5/6/2024 Posts: 4098 Rating: (193) |
follow up question published by RaviSis split to a seperate thread with the subjectWINCC professional - download graphics and WINCC project in TP1200 HMI. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
8/25/2015 1:24 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by mods315 is split to a separate thread with the subject TIA V11 SP1, no longer modify my file. Best regards |