1/26/2010 6:08 AM | |
Posts: 5 Rating: (0) |
Hi There, I am facing a strange problem in Time Synchronization.I am woking in PCS7 V7.0+SP1 and WinCC V6.2+SP2.There are 4 servers ,10 clients and 11 Automation system.We are working in WORKGROUP.Two of the servers are configured asTime Master in the WORKGRUOP(There is no external time transmitter).The whole system fully synchronized!But the problem is that the Server Clock(i.e System Time) is progressively slowing down,and along with it whole system is slowing down! Process Control Messeges are showing the server as time master.Internal system tags are also indicating the same. Please refer to the document attachedfor the configurations. Cheers! AttachmentTime Master.zip (78 Downloads) |
1/28/2010 6:10 PM | |
Posts: 5 Rating: (0) |
Has this anything to do with the lack of Server redundancy! |
Follow us on