2/23/2019 10:11 PM | |
Posts: 9 Rating: (0) |
Hi i am trying to do a home automation project. The idea is to have a plc turn on and off relays for solenoid valves for a couple garden sprinklers. I whant to change the the on and off time of the relays rather simply, the weekly timer seems perfect but my question is if it´s posible to change the weekly timers on and off values from the plc or from the logo app Ihave attatched a program in progress and if you could change the on, off and weekdays in the app it whould be complete thankful for answers! //Anton AttachmentVATTEN LOGGO.zip (194 Downloads) |
Last edited by: Anton_ma_99 at: 2/24/2019 3:00:05 AM |
|
2/24/2019 11:38 AM | |
Posts: 9 Rating: (0) |
Thaks sounds awsome! |
This contribution was helpful to1 thankful Users |
2/24/2019 1:16 PM | |
Joined: 2/22/2008 Last visit: 6/12/2024 Posts: 2698 Rating: (207) |
It would be an easy handling to integrate the unused inputs. If you add 7 switches, you are able to override the 6 timers and to force all off. The same "switches" are integrated as M1-M7 to use by the app. For addition i have add a message, because every message can only show 8 values. All counters are deleted, because you don't need it. The messages are selected with the cursor up and down keys and the override on and force off can be used directly by the switches of the inputs or the web server. See attachment with program and some pictures of the web server, if you are interested. Regards, Scorp AttachmentVatten Loggo2.zip (210 Downloads) |
2/25/2019 6:18 PM | |
Posts: 9 Rating: (0) |
Thanks realy good feedback, you learn somthing every day. |
Follow us on