1/16/2014 4:05 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating:
|
Hello! No need to convert remaining time value in DINT. Just make sure that you write this value to WORD (because it is integer) and then make sure you display it in HMI as WORD too. Just follow this simple instruction: 1. Make a temporary variable or define some MW 2. Make sure you use BI output (instead of BCD) 2. Transfer this value in HMI as word. 3. Make sure, that value format in HMI is something like 0 (instead of 0.0 or 0.00) and the lenght is actually WORD You can fine more detailed informationhere(page 167)
|
This contribution was helpful to
1 thankful Users |
1/17/2014 1:12 PM | |
Posts: 26 Rating:
|
Thank you! Solved. BR. |
This contribution was helpful to
1 thankful Users |
Follow us on