9/8/2020 4:58 PM | |
Joined: 9/23/2005 Last visit: 5/26/2023 Posts: 4184 Rating:
|
Hi, In this TIP I post a very simple WinCC Unified Performance Insight sample example. WinCC Unified Performance Insight is a WinCC Unified add-on package, that belongs to the Plant Intelligence Options (Delivery release SIMATIC WinCC Unified Plant Intelligence Options V16) . It’s used to show KPI in a comprehensive way. Downloads:
Requirements:
Documentation: There is very good information on the TIA’s Information System: Working with plant objects and plant views > Options > Optimizing processes with individual indicators Manuals on internet (SIOS):
Configuration sequence: (overview extracted from Information System, subfolder Basics > Configuration concept and from Configuring sequences (RT Unified) – clearer): Planning:
Basic settings:
In the Plant Objects (view), common data:
In the plant objects (view), Dividing the screen between Plant Objetc Types (right menu), Plant object types properties, Performance object tab and common data, performance indicators.
In screen:
In Runtime:
Sample program: AttachmentPerformance_20200903_0957.zip (490 Downloads) |
Last edited by: Denilson Pegaia at: 09/10/2020 12:18:43Denilson Pegaia |
|
This contribution was helpful to
4 thankful Users |
11/28/2021 8:26 AM | |
Joined: 1/20/2016 Last visit: 2/23/2023 Posts: 1 Rating:
|
Is it works with S7 1200 PLC |
9/8/2022 9:16 AM | |
Joined: 7/13/2021 Last visit: 5/31/2023 Posts: 1 Rating:
|
I used the example above and it works. Used software:
Follow the "Migrating V16 project" section of the manual "WinCC Unified Performance Insight - Optimizing processes with KPIs"
|
This contribution was helpful to
1 thankful Users |
Follow us on