1/10/2015 4:54 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446)
|
Hi, A new feature that STEP7 V13 SP1 brings is the use of global constants as array limits e.g. to adapt standardized data blocks to the individual application size. The so-called "Learning Mode" of S7-Graph for automatic determination of the step activation time rounds off the new version. The attached project shows a example of this feature: The block “average” calculate a simple average vale from “n” samples. “n” is a constant that defines the samples to be measured. He defines the loop limit and also the internal buffer (stat array).SP1 is available at: http://support.automation.siemens.com/WW/view/en/105825934 Attachmentaverage_V13_SP1.zip (183 Downloads) |
Denilson Pegaia |
|
Follow us on