6/13/2019 2:05 PM | |
Posts: 111 Rating: (31) |
OpennessScripter [free download] opens possibilities to automate tasks for TIA Portal. Executing a script from a Windows Batch (BAT) file, makes it possible to help field technicians. This PC automation can open, compile and download a project with minimal efforts from the field technician. This usage example is my research goal. As an assisting tool, Notepad++ [free download] can be easily customized to show code highlighting. The free OpennessScript V1.1.4. app from Siemens does not have syntax indication yet. A possible example of syntax colouring: Attached is the UDL (user defined language) definition used in the example. The Monokai style was used. I ask help from people who used OpenessScript before. Help with usage example scripts and have a look at my question topic: [PROBLEM with OpennessScripter V1.1.4 script]. AttachmentOpennessScript-UDL.zip (137 Downloads) |
Last edited by: AutoGen_1801304 at: 06/13/2019 14:06:21Last edited by: AutoGen_1801304 at: 06/13/2019 14:11:34Last edited by: AutoGen_1801304 at: 06/13/2019 14:14:53 |
|
This contribution was helpful to4 thankful Users |
6/13/2019 7:00 PM | |
Joined: 7/7/2010 Last visit: 8/27/2024 Posts: 15113 Rating: (2410)
|
Have you considered a VScode descriptor similar to the Notepad++ one? I like VScode for many reasons. I think you can launch right from VScode. Thoughts? Thanks for the contributions.
|
science guy |
|
6/13/2019 10:05 PM | |
Joined: 3/9/2015 Last visit: 8/7/2024 Posts: 34 Rating: (7) |
I think he means vsCode and making an extentions that runs your opennessScripter script directly in vsCode. |
6/13/2019 11:08 PM | |
Posts: 111 Rating: (31) |
ATT: huggy_d1 You are right. Trial download can be found: [https://support.industry.siemens.com/cs/ww/en/view/98161300]. Do you know how much the license costs? Our service gear has licenses for TIA. You have experience in this software? Is downloads only changes or is it complete replacement of the project? Diagnostics can possible be executed on tag table running on web server. Scripting for code block to open at correct place and go online could still be helpful.
|
6/13/2019 11:20 PM | |
Joined: 7/7/2010 Last visit: 8/27/2024 Posts: 15113 Rating: (2410)
|
Until 2 months ago, it was free. I have not installed a new version in the last 2 months. It replaces the entire project. ProDiag get you logic/code on the HMI (as an alternative). If I worked for a company that built, sold, installed, and supported equipment at customer sites, I would have several licenses for this tool - now that licenses are required. Or, I would at least keep using the version I have that does not require a floating licensing. If you look closely, that option still exists. Not having a license removes 2 features that you can test for 21 days, then they quite working.
|
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on