3/18/2012 5:52 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
s7200 to s71200 conversion program |
This contribution was helpful to1 thankful Users |
3/18/2012 6:17 PM | |
Joined: 9/24/2010 Last visit: 4/21/2024 Posts: 118 Rating: (10) |
I have a problem like cbcX "I ahve downloaded this tool and tried to install it but it says I need Step7 Plus 10.5 SP2 in order to install it. I already have the following installed on my machine: Step 7 Basic v10.5 SP2 Step 7 Pro v11.0 SP2 Step 7 Pro v5.5 Sp2 I have actually never heard of Step7 Plus. What's the deal with this conversion program?" I think it need TIA Portal V10.5? I think it not good because youinstall TIA Portal V11 and now you need Tia Portal V10.5 for you caninstall Convert tool 200 to 1200. It's notuseful so much. my PC and my laptop can't be runif iinstall like it need. Thank you so much
|
Mechatronic Center |
|
3/19/2012 7:02 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
http://support.automation.siemens.com/WW/news/en/58638200?Datakey=47071380 |
This contribution was helpful to2 thankful Users |
9/27/2012 3:10 PM | |
Posts: 3 Rating: (1) |
Hi Everyone, In the following link, you can download the conversion tool to convert programs in Microwin Step7 V4 (S7-200)to TIA Portal V11 (S7-1200). Hope that helps! https://www.swe.siemens.com/spain/web/es/industry/automatizacion/simatic/controladores/Documents/S7200aS71200%20Conversor.zip Regards, Sebastian |
This contribution was helpful to4 thankful Users |
1/9/2014 5:06 PM | |
Posts: 3 Rating: (0) |
Thầy Hiếu cho em xin link down Tia Portal V10.5 nhé, em muốn chuyển chương trình s7-200 sang S7-1200 mà TIA v12 làm không được. Cám ơn thầy nhiều. |
1/10/2014 8:35 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Hello Votrongnguyen please write your post here in english, because this is the spoken language of this part of the forum. Best regards O_Moderator |
1/11/2014 7:11 AM | |
Posts: 204 Rating: (29) |
Hello First Convert the program from s7-200 to the TIA v10.5 and then migrate it the TIA V11. hope this helps. |
6/4/2014 4:16 PM | |
Posts: 2 Rating: (0) |
This link doesn't seem to work anymore. |
6/4/2014 5:58 PM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715) |
Hello, The link is working but it leads to another tool Try this one: S7200- to S7 1200 converter Regards, Marcjan |
Problem solved? |
|
Follow us on