5/2/2018 2:21 PM | |
Joined: 6/30/2014 Last visit: 7/8/2024 Posts: 457 Rating: (87)
|
Hello dear, I'm not sure if I understand your issue right, but (with the delivered information until now here), I would suggest the following steps if I were you: -- > I would use COMOS (at best with version 10.2.2) to open that files -- > I would rebuild the issue can create a log file with the DebugView,(Link->) here you see how that works -- > In case it persists, I would open a (Link ->) ticket at Siemens, if I were sure that they should check the behavior of the software; in that case, I would deliver as much information and files as possible. On the other hand, you could provide us at this forum with all the needed information and files, to see if we can help... it is up to you, which road you prefer to go. All the best, SuperPippo |
5/7/2018 10:49 AM | |
Joined: 4/9/2018 Last visit: 11/10/2022 Posts: 72 Rating: (31) |
Thanks for your input, I'm in contact with Siemens via GTAC, I'll first see what they can do. |
Follow us on