12/9/2024 2:10 PM | |
Joined: 1/30/2023 Last visit: 12/16/2024 Posts: 11 Rating: (0) |
Hi Duris, in my configuration HMI TP1500 is the master of modbus TCP/IP communication, today i connect again my HMI Panel at the Prosafe interface and did test again. Same result of the first one. in the attachment i add a new wireshark scan without exception response, how i set the HMI tags and a little video of my online PLC (Prosafe) that i force a value on it and the HMI waiting time before update the value. i don't have much options on Prosafe PLC because i need to follow the default columns of datas, all the signals work, both side, but that a lot of time to animate the graphics. in the video in attachment, i force at 25.0% the value of AI-55001, before i see this value on HMI it's visible the H, means that PLC send High threshold before see the value (High threshold set is 20.0%) Thank for every reply AttachmentLocal_Test.zip (12 Downloads) |
Follow us on