1/17/2023 10:55 AM | |
Joined: 8/3/2009 Last visit: 10/14/2024 Posts: 13919 Rating: (1757)
|
Hello sixthomas to test with a "clean" Panel you could do a Reset with factory settings with the Panel. Then work with the latest Image Version on the Panel that is available for yoru TIA Portal Version. Check also if you have logging (alarms or tags). the TP1200 has only 20000 entries for on entire log. Do not use bigger values for this, this could cause performance problems. you could also use Option+ to display the panel performance values to see if the panel runs in overload or if its just a communication issue with the PLC. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on