6/15/2010 6:39 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, You can use the following RS232/PPI Multi Master cables for downloading a project: Order Number: 6ES7901-3CB30-0XA0 The RS232/PPI Multi Master cable (with 8 DIP switches) can be used if DIP switch number 5 is set to PPI/freeport ("0"). The cable must be dead for it to accept the change. Look at How do you backup/restore with a Windows-based panel? (baud rate best regards, Hristo Mihalev |
6/19/2010 11:23 PM | |
Joined: 5/28/2008 Last visit: 4/8/2025 Posts: 4520 Rating:
|
Hello Simon Wales, No, It's not possible to lock the HMI in order to disable backup function. I think that the problem is in the connection. Please have a look on this FAQ to chose the suitable transfer option to you What transfer options are available in the various operator panels? Regards. |
Ayman Elotaify |
|
8/13/2015 3:18 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by manoz is split to a separate thread with the subject Backup from existing TP177A HMI and download to new TP177A by Prosave V9.0.3.0. Best regards |
Follow us on