6/22/2015 8:45 PM | |
Posts: 36 Rating: (1) |
Hello, how do i send a program, like an exell file from my computer to my TP700 comfort panel? thank you |
6/23/2015 8:38 AM | |
Joined: 8/3/2009 Last visit: 8/6/2024 Posts: 13467 Rating: (1704) |
Hello Fredmans You cannot get a direct access to the filesystem of a Simatic Panel. The only posibillity is to use the Miniwebsites of the Panel (activate Option Webpages; has nothing to to with Sm@rtServer). With a login in the Webpage o nthe Panel you can click toa file system browser an get a manual access to the files on the Panel or the External storage devices. You need to run the Websites a Sm@r Service License (in WinCC flexible) but for testing it works without license. In TIA Portal the Websites can be used without License! The other Way ist to get Access from the Panel to a storege Device of another PC in the Network Look at this FAQ: https://support.industry.siemens.com/cs/ww/en/view/92346478 I hope this helps Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on