12/21/2014 10:39 PM | |
Joined: 12/13/2014 Last visit: 12/11/2023 Posts: 1 Rating: (0) |
Hello, I'm trying to send a http:// command with my cpu. Is this possible? In my lan i have a serverwhere i want to send a command to. I tryed to connect with t_con but i don't get a response. an example of the command: http:// ipaddres:port/json.htm?type=command¶m=switchlight&idx=6&switchcmd=Off&level=0 I hope somebody can help me. Thanks
|
Last edited by: Min_Moderator at: 12/22/2014 12:06 PMSplitted |
|
12/22/2014 1:22 PM | |
Posts: 1368 Rating: (126) |
Hello, first of all: I haven´t done it before, it is just an idea... So...do you know the application with snmp http://support.automation.siemens.com/WW/view/de/57249109 in this application, the SNMP protocol was cloned and then send by TSEND. Perhaps you have to do this also with the HTTP GET/REQUEST.... Therefore, you can look with e.g. wireshark how the HTTP protocoll is constructed. Just an idea... |
Follow us on