2/9/2013 4:04 AM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello chris; I am afraid that the temporary variable is the way to go. Look at the program example attached below, taken from the FBD manual: SIMATIC STEP7 V5.5 Function Block Diagram (FBD) for S7-300 and S7-400 Programming Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
2/9/2013 6:27 AM | |
Posts: 8 Rating: (1) |
HiDaniel, Thank you for answering my question. I appreciate it.
|
2/9/2013 12:49 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684) |
Hello chris; The manual I proposed earlier was for Simatic Manager, I just saw that you posted in the TIA Portal section. In caseyou develop doubts about the answer based on the programmingplatform, here is the same example FBD code published in the TIA Portal manual: STEP 7 Professional V11.0 SP2 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
2/9/2013 7:30 PM | |
Posts: 8 Rating: (1) |
Thanks,Daniel. I did notice the slight difference between the programming platforms but the basic ideas are the same. |
11/18/2021 7:40 PM |
|
Joined: 11/1/2021 Last visit: 9/3/2024 Posts: 11 Rating: (0) |
Hi The example you shared is for LAD the main question is related to FBD not LAD. Regards |
Follow us on