5/11/2015 3:53 PM | |
Posts: 2 Rating: (0) |
The Backup Project Has been done in 2012 with Starter V4.2. HF1 Hardware is GL150 CU320-2-DP V4.4 Today I try to open my backup project with Starter V4.4 HF3 and even if the SSP Sinamics MV V4.4 SP2 is installed. There is no possibility to open the project, Maybe because of SP2.(check pdf doc) Impossible to find SSP Sinamics MV V4.4 only. Software Starter V4.4 HF3 is compatible with all Old Firmware ? How Can I Go Online with the version V4.4 HF3 on the GL150 CU320-2-DP V4.4 if the SSP is not correct Should I have to use The Starter V4.2 HF1, which one is not available anymore ?
Thanks for your Answers
Lionel I&C engineer
AttachmentStarter Info.pdf (353 Downloads) |
8/11/2015 4:54 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by gabbar is split to a separate thread with the subject MM440, communication with STARTER. Best regards |
Follow us on