3/9/2015 4:03 PM | |
Posts: 3 Rating: (0) |
Dear ALL I,ve got 3 independent machines each one is equipped with: 1st machine 135U CPU. 2nd machine 135U CPU. 3rd machine 95U CPU. 1 DOS computer were STEP5 V6. and were DOS6 installed. I can go online with ALL CPUs without any problem. On windows XP PC service pack 1 I’ve install STEP5 V7.2 from CD (No problem during installation ) Communication with U95 CPU is OK Communication with U135 CPU is NOT ok Undefined characters from AS I use s5as511.exe from: https://support.industry.siemens.com/cs/document/11870684?pnid=14395&lc=en-WW Communication with U95 CPU is OK Communication with U135 CPU is NOT ok Undefined characters from AS I reinstall the STEP5 V7.2 again I update it to V7.23 from: https://support.industry.siemens.com/cs/document/18177672?lc=de-WW Communication with U95 CPU is OK Communication with U135 CPU is NOT ok Undefined characters from AS I install the s5as511.exe from: https://support.industry.siemens.com/cs/document/11870684?pnid=14395&lc=en-WW Communication with U95 CPU is OK Communication with U135 CPU is NOT ok Undefined characters from AS can you help me to solve this problem aarb
|
Follow us on