9/30/2022 7:01 AM | |
Joined: 6/27/2018 Last visit: 3/28/2024 Posts: 16 Rating: (0) |
Good morning, Is it possible to access to unified web page (my op project) withouth login and password? |
9/30/2022 7:18 AM | |
Joined: 2/17/2020 Last visit: 5/13/2024 Posts: 1001 Rating: (171) |
Hi ErosMch1, Maybe you are looking for the Autologin to the Unified project? Please see. WinCC Unified V16: Auto login browser extension for google chrome Note: DerHecht4.0 is a user who has developed numerous step-by-step Unified examples and configurations in video format that I believe are very useful and interesting, so I recommend you take a look at his profile. |
A rating will be well appreciated. |
|
This contribution was helpful to2 thankful Users |
11/20/2023 12:57 PM | |
Joined: 11/28/2022 Last visit: 3/20/2024 Posts: 21 Rating: (0) |
Hello, I update this issue. I have the same behavior described in the Siemens knowledge base. Do you know if there is a solution to fix this issue in v19 ? Siemens Knolewdge base : Note
Login and logout behavior with WinCC Unified PC Runtime Note that "Automatic login with login data" doesn't work too on a client over the network. |
Last edited by: Jen_Moderator at: 11/21/2023 08:34:59Link optimized. |
|
11/20/2023 2:21 PM | |
Joined: 1/21/2013 Last visit: 5/13/2024 Posts: 2767 Rating: (448)
|
Hi, As far as I know, WinCC Unified PC Runtime V19 will come with a feature called "My WinCC Unified", which will allow to define client-specific rules (define start screen, define screen resolution, configure auto-login/logout). However, this will require a static IP address for the client and the auto-login will not allow to specify a user, it will be as described in 2.2 Automatic login without login data. Kind regards |
This contribution was helpful to2 thankful Users |
Follow us on