3/29/2013 4:11 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating:
|
Hello , If you are using STEP7 for S7300 and s7400, you have option of monitoring effect of mentioned input "DI0.4" on "DB6.DBW38" by using variable tables.Other PLCs also have the capability to monitor the internal variables. If you are sure that this change happens, trace the logic for possible inadvertent writing values.Also check the following topic for a detail discussion to trace variables in S7 program: indirect adress tracking Best regards Hamid Hosseini |
Last edited by: hdhosseini at: 3/29/2013 4:18 PM |
|
This contribution was helpful to
1 thankful Users |
4/1/2013 7:27 AM | |
Posts: 7 Rating:
|
u will have to use area pointer for that. |
4/3/2013 2:01 PM | |
Posts: 3037 Rating:
|
Hello ASTECH, Yes this is good, if you post the solution for your problem. Tweety |
Follow us on