11/8/2010 5:16 PM | |
Joined: 1/4/2007 Last visit: 5/6/2024 Posts: 1117 Rating: (174)
|
Hello Fazal, To your questions: Siwarex: 1. The Siwarex FTA module has 8 digital outputs. You can define a functionality for each of these 8 digital outputs, e.g.: - Coarse signal - Fine signal - Limit value for overloading You can achieve this, by setting the parameters of the Siwarex FTA module into the “DR7” / “Digital outputs” of the Siwatool software. If you don’t have the Siwatool software, you can download the demoversion on the internet: http://support.automation.siemens.com/WW/view/en/18788325 With that demoversion, you can “play” a little bit into your office. 2. The Siwarex FTA module doesn’t need the junction box 7MH3710-3AA. The Siwarex FTA module needs only the 3 load cells and one of the two junction boxes for connecting the load cells in parallel: - SIWAREX JB, aluminum housing: 7MH4710-1BA (see also the pdf-page 63 of the attached file) - SIWAREX JB, stainless steel housing: 7MH4710-1EA (see also the pdf-page 65 of the attached file) S5-S7 communication: 1. Well, if you are using a S7-300 along with a Siwarex FTA module, the S7-300 PLC has full access to the Siwarex FTA module, also to the setpoint.But I don’t know, if S5 supports Ethernet. Profibus-DP is working! 2. As mentioned, you have full access to the Siwarex FTA module with the S7-300 PLC. But I don’t know, if S5 supports Ethernet. Best regards Siwarexi AttachmentWT10_2010_en_Kap03_load_cells.pdf (119 Downloads) |
11/10/2010 3:59 PM | |
Joined: 1/4/2007 Last visit: 5/6/2024 Posts: 1117 Rating: (174)
|
Hello Fazal, Well, there is no way to export the data to the Siwarex FTA module, because both modules are completely different! I recommend you to do the adjustment as described into the attached file. (If you have questions to the procedure, you can ask me) If you want, you can read the dosing parameters from the Siwarex S module to the S5-PLC. But I have no experience how to do this… Ask your customer for the following dosing parameters, so you can set these parameters correctly into the Siwarex FTA module: - set weight of the dosing (DR20 into Siwatool) - Trailing weight (DR22 into Siwatool) - Fine weight (DR22 into Siwatool) These are the most important parameters for a dosing. Best regards Siwarexi AttachmentSIWAREX_FTA_Quick Guide _V3.1.pdf (183 Downloads) |
10/8/2013 6:48 PM | |
Posts: 1 Rating: (0) |
Hallo Fazal The Parameter from the Siwarex S are all in one Datablock. You can transfer this Datablock with Siemens Step 5 Program. In the Attachment you can find the Manual. In this Manual you can find all Parameter from the Siwarex S. With best Regards MISJO Sorry the Manual was to big. Only the Parameter in the Attachment. AttachmentParameter_Siwarex_s_handbuch_e.pdf (123 Downloads) |
Follow us on