3/22/2016 9:17 AM | |
Joined: 6/21/2013 Last visit: 7/27/2022 Posts: 13 Rating:
|
Hi Oreca! I'm from Viet Nam. At the moment, my company is using DCS sytem with program software is PCS7 V7.1.sub software is Cemat. The programs has edited by CFC language. Now we want to upload program from PLC S7-400 to PG. But we don't how, can you guide us? Thanks you! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/22/2016 4:01:41 PMNew subject after splitting |
|
3/22/2016 10:09 AM | |
Joined: 3/14/2008 Last visit: 8/16/2024 Posts: 2086 Rating:
|
Hi vukhiem, PG you mean your ES station? In this case, you will need to execute a readback of the CFC program online of the CPU (see my previous post how to do this). Default is OCM parameters, which are the parameters an operator or engineer can change, like timer values, parameters at a analog value. You can use all parameters, but I only do this when I migrate a project. Furthermore, if you have user archives, you can do an export of the user archives of all servers. For this, you have to go to you WinCC explorer and open the "User archives". In there you can execute a export of all your archives (one at a time). |
Last edited by: Oreca at: 3/22/2016 10:10:59 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
3/23/2016 10:57 AM | |
Joined: 3/14/2008 Last visit: 8/16/2024 Posts: 2086 Rating:
|
Hello, OK, let's go back to basics....What is your setup? ES, OS server, Client? I don't know what you want to achieve by uploading program to PG. In your last post, you are not talking about an engineering station as PG are you? As Myst told you, you cannot do that. When you do a readback to an ES station, the CFC program is compiled fully, but afterwards you can do a download change (since your offline blocks have changed). So I don't know what you did exactly to cause the PLC to be downloaded fully? Can you give us some screens. You can compare the blocks in the CPU with the CFC program: Go to the CFC editor and select CPU->Compare or select the S7_program folder->Charts and right click to select CPU->Compare. |
If I could help you, you can use the RATE button. Thank you. |
|
3/23/2016 3:48 PM | |
Joined: 6/21/2013 Last visit: 7/27/2022 Posts: 13 Rating:
|
Hi Oreca! Our Sytem use for control a cement assembly line, the sytem have 7 clients, 1 Sever, 1 standby, 1 ES. PCS7 and cemat software is installed in Es. this promblem is when our engineer make an archive then ES PG appear error him force reset ES PG by hand. After, he strart again ES PG and open multi pro but all stations were lost only have Library master. next, he retrieve file archive. and now, we can't online. we only online hardware configuration. You told exactly, with ES PG we only need compile the firtstime, after we can download changes only. but at the moment, ES PG allow compile changes only, but when we want online then program don't allow. when we want to download program then can't select download changes only or entire program. Now our company can't stop, so we can't check everthing. Because, during process sometime any fault occur and we need online to check fault where sometime we have to unlock interlock. but now we can't. So, We hope everyone can help us. Thank you! AttachmentFull page photo.pdf (276 Downloads) |
Last edited by: vukhiem at: 3/23/2016 4:05:14 PM |
|
3/23/2016 4:06 PM | |
Joined: 6/21/2013 Last visit: 7/27/2022 Posts: 13 Rating:
|
result and "select the S7_program folder->Charts and right click to select CPU->Compare." sameAttachmentFull page photo.pdf (251 Downloads) |
Last edited by: vukhiem at: 3/23/2016 4:08:51 PM |
|
Follow us on