10/16/2014 1:59 PM | |
Posts: 84 Rating: (0) |
Can anybody help me? |
10/21/2014 11:45 AM | |
Posts: 457 Rating: (46) |
Hello Jengeese, please see this link regarding dynamic setting of monitoring limits: http://support.automation.siemens.com/WW/view/de/27062514 If changing of limit values cannot be done directly you have to change alarm behavior to "triggered by bit" (if a bit gets HIGH then an alarm appears) . These bits (local tags) will be set and controlled by your own VBA/C function where you provide limits and calculate them. Please read above link and refer to it if you don't get the solution. Maybe some jpegs will help, too. Georg |
11/6/2014 12:19 PM | |
Posts: 84 Rating: (0) |
Thank you so much, I thought that before too however I am so new and I don't know how to accumulate the old value of them. Can you help me for this too? |
11/6/2014 2:19 PM | |
Joined: 2/21/2014 Last visit: 3/14/2024 Posts: 652 Rating: (344) |
Hi Jengeese, I don't know how to read DB values in SCL. therefore i have created an exmaple with input fields only. anyways you just need the the logic, so i think this should be enough for you. please see the attachment. it's SCL code. Attachment\\BLRKAPT0002nas\PCS7_Library\DELETE\Harry\Test.zip (63 Downloads) |
You can always use "Rate" and "To Thank" button to appreciate my efforts in helping you :) |
|
Follow us on