6/23/2015 12:22 PM | |
Joined: 11/9/2008 Last visit: 7/1/2024 Posts: 404 Rating:
|
Hi All, For my PLC control panel I want select UPS and Transformer.Transformer is step down from 230 VAC to 110 VAC. I have 4 no.of 10 A power supply(SITOP PSU100L 24V/10A 6EP13341LB00). Input Current ● at rated input voltage 120 V 4.1 A ● at rated input voltage 230 V 2.4 A ● inrush current 65 A Output Current Rated current value Iout rated 10 A For Calculation of UPS and Transformer I just need to add power supply input current only? is it right?or I have to add input and output current of power supply? Whether I need to add inrush current also? Please help to understand this. If possible please give some example. Regards, Yogendra G
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/23/2015 4:56:39 PMNew subject after splitting |
|
Follow us on