5/24/2017 9:45 PM | |
Joined: 5/30/2013 Last visit: 7/7/2024 Posts: 112 Rating: (37) |
Hi Nutarharion, maybe help this FAQ for much better understand pointer. Programming a Loop with Indirect Addressing For the end there are a some posts: S7 300 Function for filling DB of value Need help in indirect addressing of FB Stat array More information: https://support.industry.siemens.com/cs/search?lc=en-WW DBzz: WORD; ZZpointer: DWORD; LoopNu: INT; pet: INT; L #DB_ZZ // load Data Block number L P#0.0 L #ZZvalue Best regards zzVss |
Last edited by: zzVss at: 5/24/2017 10:32:32 PMLast edited by: zzVss at: 5/24/2017 10:35:34 PM |
|
This contribution was helpful to1 thankful Users |
5/25/2017 1:06 PM | |
Joined: 5/30/2013 Last visit: 7/7/2024 Posts: 112 Rating: (37) |
It is pleasure to help you.. Best regards zzVss |
5/26/2017 7:48 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Nutaharion, U should use SCL language for more ease and freedom for array related pointers application. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on