3/24/2024 5:10 PM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
this message come up if the settings of the USB Adapter not match the bussettings online. Which settings you use ? |
3/27/2024 7:49 AM | |
Joined: 1/1/2017 Last visit: 7/22/2024 Posts: 331 Rating:
|
Hello Christoph, Device USB\VID_0908&PID_0004\6ES7_972-0CB20-0XA0 was configured. Driver Name: oem60.inf Class Guid: {745a17a1-74d3-11d0-b6fe-00a0c90f57da} Driver Date: 11/06/2019 Driver Version: 9.2.5.0 Driver Provider: SIEMENS AG Driver Section: PCAdapter_Device Driver Rank: 0xFF0001 Matching Device Id: USB\VID_0908&PID_0004 Outranked Drivers: Device Updated: false Parent Device: USB\ROOT_HUB30\4&3a727aa6&0&0 Device USB\VID_0908&PID_0004\6ES7_972-0CB20-0XA0 was started. Driver Name: oem60.inf Class Guid: {745a17a1-74d3-11d0-b6fe-00a0c90f57da} Service: s7oupc2x64 Lower Filters: Upper Filters: Device settings for USB\VID_0908&PID_0004\6ES7_972-0CB20-0XA0 were migrated from previous OS installation. Last Device Instance Id: USB\VID_0908&PID_0004\6ES7_972-0CB20-0XA0 Class Guid: {745a17a1-74d3-11d0-b6fe-00a0c90f57da} Location Path: Migration Rank: 0x0 Present: false When I tried to reinstall the driver from the supplied CD, this error displayed: AttachmentPC Adapter USB A2 Login Authorization Error.mpeg (204 Downloads) |
Last edited by: OMKRIS2017 at: 04/02/2024 07:49:58Last edited by: OMKRIS2017 at: 04/02/2024 08:46:15 |
|
4/2/2024 5:51 PM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
activate the option "only master on the bus" and thrn try it again |
Follow us on