6/12/2020 6:35 PM | |
Posts: 12 Rating: (0) |
Hello, Does anyone know which other USB transfer cable works with TP177B mono DP than the ones recommended in the attached PDF file. The recommended cables are unavailable. Thanks Liston Attachmentusb_transfer_v1_0_e.pdf (185 Downloads) |
Last edited by: Liston at: 06/12/2020 18:35:59 |
|
6/12/2020 6:47 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820)
|
Hello, reason use that USB special cable? |
With best regards... |
|
6/12/2020 7:21 PM | |
Posts: 12 Rating: (0) |
To transfer, backtransfer and backup project from TP177B |
6/12/2020 7:28 PM | |
Posts: 12 Rating: (0) |
The other port is RS485 which is connected to S7200( also HMI is powered with the same cable). Unfortunately there is no ethernet. So USB is my only option. |
6/12/2020 7:45 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820)
|
Hello, eeeeehm ok |
With best regards... |
|
Follow us on