3/9/2015 8:11 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2146)
|
Hello Samnina, I do not understand what really your problem is. The Userarchive is an option of WinCC. You have to select it during installation, because it is not installed per default. If it is installed, you have the Userarchive-Editor in WinCC-Explorer. To start the Userarchive-Server, you have to set the "hook" in the Startuplist in the Computer-properties. The Userarchive-Server can run on WinCC-Servers or Single-Stations. You can check, if the process "CCUsrAcv.exe" is running in Runtime. If not, it may have crashed. In this case you should create a userdump, see https://support.industry.siemens.com/cs/ww/en/view/45020870 If you would have an userdump, you can create a Support Request and send it to the Technical Support. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
6/28/2017 2:20 PM | |
Joined: 6/19/2017 Last visit: 5/15/2024 Posts: 8053 Rating: (164) |
New question published by eric47800 is split to a separate thread with the subject Migrate WinCC7.0 to WinCC7.4 - the script for UA have the error 1004 . Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on