5/18/2006 8:22 AM | |
Posts: 3149 Rating:
|
Hi, this issue has already been discussed: /tf/WW/en/Posts/2826 >If no one is logged in when the alarm occurs, no username is displayed for Comes In, >Acknowledged, or Went Out. This happens even when you have to be logged in to Ack. or >clear an alarm. I guess, that you are using the tag@currentuser for your purposes? => this tag will have no entry, if no one is logged in. http://support.automation.siemens.com/WW/view/en/22269581 http://support.automation.siemens.com/WW/view/en/19700833 What about using WinCC audit/SIMATIC logon? http://support.automation.siemens.com/WW/view/en/19300590 nemo |
6/19/2006 9:41 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Nice solution [:D] Thanks for posting |
Follow us on