8/17/2011 10:23 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
|
8/17/2011 4:00 PM | |
Joined: 9/27/2006 Last visit: 5/27/2024 Posts: 12257 Rating: (2668)
|
Hello Navnag; OSCAT.de proposes a solution also for handling double-precision REALs in S7 CPUs: 8. Arithmetics with Double Precision 8.1. Introduction Floating point numbers are stored in the format REAL. A common data format according to IEC754 used a 24 bit wide mantissa and an 8-bit exponent. This results in an accuracy of 7-8 digits. Usually this is for applications in control technology more than sufcient, but in certain cases can lead to a problem. A typical case can which be solved with single-precision only inadequate is a consumption meter. If you want to several Mwh (megawatt hours) of total consumption adding up, taking a smallest power of 1 mW (milliwatt) at a distance of 10ms fairs and so you need a resolution of 3.6 * 10^7 (equivalent 10MWs) and it would be a do add up 1* 10^-5 W's. To do this it requires a resolution of 12 digits. The solution implemented by OSCAT is REAL Double precision and has a resolution of about 15 digits. The implemented data type REAL2 consists of R1 and RX, RX is here the value saved the first 7-8 points as Real and the rest in one real R1. This data type has the advantage that no conversion of REAL2 to REAL is needed, rather, the RX is rather part of single REAL value. Attachmentoscat_basic_doc_332_DouleReal.pdf (1773 Downloads) |
This contribution was helpful to4 thankful Users |
11/28/2011 4:19 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
How can you process 64-bit floating-point numbers in STEP 7 V5.5 with a SIMATIC S7-300/400 CPU? |
This contribution was helpful to6 thankful Users |
5/18/2015 2:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|
This contribution was helpful to1 thankful Users |
Follow us on