4/23/2019 7:15 AM | |
Posts: 8 Rating: (0) |
Yes. I want to Limit the preset value of Timer, which is failsafe timer. I want to set Minimum limit for that Timer. earlier we used block which is available in normal FC you can see that image in link. same block is not available in Failsafe FC also less than equal to followed by move is also not getting accepted. [snip] I WAS UNABLE TO UPLOAD IMAGES SO I UPLOADED AND SENT LINK.
Attachmentfailsafe program pics-20190424T053251Z-001.zip (87 Downloads) |
Last edited by: Jen_Moderator at: 4/24/2019 7:33:25 AMRemoved link and added file as an attachment. |
|
5/7/2019 11:15 AM | |
Posts: 8 Rating: (0) |
I am not able to optimize safety datablock. how did you optimized? |
Follow us on