2/17/2020 5:37 PM | |
Joined: 8/25/2014 Last visit: 2/12/2025 Posts: 133 Rating:
|
Hello. Has anyone tried this communication, Is there any lag between when turning the drive on and off. I would like to change speeds of the drive so that a workpiece comes into position based on the inductive switches. It doesn't need to be 0.1 mm accurate, but still as accurate as possible. So the response from the drives should be quite fast... I will have two drives on the USS network... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/18/2020 05:46:26New subject after splitting |
|
Follow us on