8/7/2019 7:46 AM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (790)
|
Hello, if this is a 60Hz motor you have to check that your reference frequency in p2000 is set to 60hz. In case you just want to run a motor with nominal 50Hz at 60Hz you can adapt the scaling of your analog input so you can provide setpoints from 0 to 60Hz which are equal to 0% to 120% on a 50Hz reference. You can also check out r0755 in the V20 operating instruction manual for detailed information about the scaling of the analog input https://support.industry.siemens.com/cs/ww/en/view/109768394 |
With best regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on