2/12/2019 4:02 PM | |
Posts: 31 Rating:
|
Hello, I have a V20 VFD and I want the drive to use a full speed setting (60Hz) unless digital input 3 is on and then I want the drive to use a programmed fixed frequency. I am trying to figure out P1000. I need help with determining which selection to use. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/13/2019 9:42:52 AMNew subject after splitting |
|
2/13/2019 11:28 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello, |
With best regards, |
|
2/13/2019 3:19 PM | |
Joined: 3/27/2008 Last visit: 7/11/2024 Posts: 1123 Rating:
|
Does this help. select the two speeds as required. Also P1080 will have to be increased to 60Hz to allow the higher speed.
AttachmentV20 2 speed connection..pptx (155 Downloads) |
Last edited by: tractor at: 2/13/2019 3:35:19 PMTractor |
|
2/14/2019 6:03 PM | |
Posts: 31 Rating:
|
I will give these a try. Thank you |
Follow us on