4/1/2022 9:58 AM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191)
|
Hi Riis82, APL and IL work perfectly together. Both are subject to the same quality requirements and are tested extensively, also together, by the Siemens system test. The industry library is the result of the merger of several industry add-on libraries ( e.g. water library, semiconductor library) and was added to the official standard portfolio. The sales release summarizes very well the added value of the IL compared to the APL: |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
4/1/2022 2:15 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi Thunderstorm, The blocks added since IL V9.0 SP1 have some issues. These are blocks from BRAUMAT like adapter blocks, Unitif, EqmIf, BatchIf. The blocks are not aligned completely with APL blocks and with the new EPHT/EMT concept. We have created the necessary workarounds for them, but good news is that these issues will be fixed with IL V9.1 SP1...so hopefully it is released soon
|
Last edited by: Oreca at: 04/01/2022 14:36:07If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/1/2022 2:32 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, To answer your question: The VlvDiv and VlvDsL blocks are working fine, the IL has been out there since V8.0 so it has been out there a while. But some blocks that were added since V9.0 SP1 lack some functionality. Overall the IL is a good addition to APL, but I think Siemens has released V9.0 SP1 to soon, because the mentioned blocks need work.
|
Last edited by: Oreca at: 04/01/2022 14:39:07If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/6/2022 4:50 PM | |
Joined: 10/26/2011 Last visit: 10/1/2024 Posts: 762 Rating: (191)
|
Hi, The Indsutry library was released on 12/23/2021 and should have fixed all the mentioned bugs except for the mentioned ones regarding Braumat blocks. The IL V9.1 is compatible with PCS 7 V9.1 and V9.1 SP1. |
Last edited by: Thunderstorm at: 04/06/2022 16:51:58SIMATIC PCS 7 - Overview |
|
Follow us on