6/11/2015 7:41 AM | |
Joined: 5/7/2015 Last visit: 9/20/2024 Posts: 20 Rating: (1) |
Hi all, please - I am totally rookie with siemens (except LOGO) and I am trying to connect VIPA 313sc 5BF03 (many times used, because it is piece for learning) with my pc (TIA v13) using ethernet cable. I found few instructions how to set up PG / PC interface etc. but almost everything is in S7 5.x. But anyway...I tried to do it in TIA and I can see my unit in Accessible devices and I can assign IP address (ping is working few seconds and after that "IP address could not be assigned") but when i am trying to download program, TIA shows me "Configured access nodes of PLC_1" where is Type MPI and my choices for PG/PC interface are only MPI, Automatic protocol detection and Teleservice. Maybe i have wrong config of PG/PC interface? You can see it in screenshots. Or I need MCC even if power for unit is ON all the time? Again - I am totally rookie so please be gentle to my stupidity and my english too Thanks a lot for every answer!!!
Attachmentscreenshots.zip (284 Downloads) |
6/11/2015 7:51 AM | |
Posts: 5225 Rating: (1192) |
VIPA is not from Siemens. |
6/11/2015 8:37 AM | |
Joined: 5/7/2015 Last visit: 9/20/2024 Posts: 20 Rating: (1) |
Message received I am searching on VIPA site right now... Thanks for help guys! |
Follow us on